Digital Input


What you will find in this section:

  1. Digital input

 

The digital input complies with IEC 61131-2 Type 3. It includes the following functions:

  • Impulse counter
  • Tariff selection
  • Synchronization of average values
  • Acknowledgment of alarms

 

Digital input

 

Digital input
Digital input

 

Status

The “Status” area shows the current status of the digital input.

Linked functions

The digital input has been configured with a defined function.

By clicking the respective link, you can access the configuration page for the function.

Settings

An identifier can be assigned to the digital input. With the checkbox, it can be activated or deactivated.

In the default settings, the digital input is activated.

 

 


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history